AXIS#.VL.ARZQ1 TO AXIS#.VL.ARZQ4
Description
AXIS#.VL.ARZQ1 sets the Q (quality factor) of the zero (numerator) of AR filter 1. This value is QZ in the approximate transfer function of the filter:
AR1(s) = [s²/(2πFZ)²+s/(QZ2πFZ) + 1]/ [s²/(2πFP)² +s/(QP2πFP) + 1]
The following block diagram describes the AR filter function; note that AR1 and AR2 are in the forward path, while AR3 and AR4 are applied to feedback:
AR1, AR2, AR3 and AR4 are used in velocity and position mode, but are disabled in torqueTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist mode.
Discrete time transfer function (applies to all AR filters)
The velocity loop compensation is actually implemented as a digital discrete time system function on the DSP. The continuous time transfer function is converted to the discrete time domain by a backward Euler mapping:
s ≈ (1-z-1)/t, where t = 62.5 µs.
The poles are prewarped to FP and the zeros are prewarped to FZ.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
0.1 to 5 |
Default Value |
AXIS#.VL.ARZQ1: 0.707 VLARZQ2 to VLARZQ4: 0.5 |
Data Type |
Float |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus![]() |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT![]() |
AXIS1.VL.ARZQ1 | 0x5011 | 0x1C | UDINT | 1000:1 | - | RW | False |
AXIS1.VL.ARZQ2 | 0x5011 | 0x1D | UDINT | 1000:1 | - | RW | False | |
AXIS1.VL.ARZQ3 | 0x5011 | 0x1E | UDINT | 1000:1 | - | RW | False | |
AXIS1.VL.ARZQ4 | 0x5011 | 0x1F | UDINT | 1000:1 | - | RW | False | |
AXIS2.VL.ARZQ1 | 0x5111 | 0x1C | UDINT | 1000:1 | - | RW | False |